EGEAR.ON

Description

The command EGEAR.ON starts the electronic gearing procedure according to the selected electronic gearing mode:

Mode Description
0 Gearing Off
1 Gearing On

Change this parameter only when the motor is not moving (MOVE.MOVING = 0). If you attempt to make a change while the motor is moving, an F826, "Cannot execute during a move" fault is produced.

General Information

Type

Command

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

Start Version

N/A

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1068

No 8 bit No

M_01-05-11-000

Related Topics

Electronic Gearing